This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq2031 inductor selection

how do i determine the dc resistance that is required for the inductor that i have used. this is the specification of my design.

I have used the two step algorithm for a 24volt battery with 12 cells.

Vdc - 37.28V

Imax - 2.5A

 

 

 

l

  • The DC resistance simply affects the efficiency of the charger and is arbitrary.  Usually, there are size constraints for the charger system which limits the DCR to some level.  A lower DCR will give a more efficicient charger.

  • Hi Arun,

     

    Can you please post your circuit or the resistor values that you used to make the 24V charger. I would like to compare them.

     

    I'm looking for a circuit on which changing a jumper will charge a 24V Battery and default is 12V SLA battery.