This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2596S-ADJEVM: Current Limiting Protection

Part Number: LM2596S-ADJEVM
Other Parts Discussed in Thread: UCC39002, LM2596

If load of motor connected to output has max stall torque current of 4.2A, will current-limiting protection cause this chip to shutdown at 3A before it is damaged?

Also, can output of two of these chips be combined to provide more current?