This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ31710: Output capacitors

Part Number: LMZ31710


Hello,

Our customers use the following capacitor in parallel as an output capacitor of the LMZ31710.

These are different from the recommended capacitors.

Are there any problems?

・T520D687M004ATE012(KEMET)  680uF ±20%,ESR 12 mOhms (100kHz 25C),T520
・C3225X5R1A476M250AC(TDK)   47μF ±20%,ESR 2.4mOhms (100kHz),X5R
・C1005JB1A105KT(TDK)                  47μF ±20%,ESR 2.4mOhms (100kHz),JB
・C1005JB1H104K050BB(TDK)        100nF ±10%,ESR 227mOhms (100kHz),JB

Vin=5V,Vout=1.05V

Best regards,
Seishin