Other Parts Discussed in Thread: TPS63024, , TPS63050
Tool/software: WEBENCH® Design Tools
I did not find any designs in webench for the TPS63036. I did find designs for the TPS63024 and TPS63050 parts. I understand TPS63050 is a newer part (than the 036) but do like to use Webench for quick efficiency calculations and also appreciate the fast-track design with parts already suggested - although I use these as general guidance more than anything else.
My interest in the part is:
... which shows of the 3 regulators, the TPS63036 has the lowest Iq, allows for the lowest switching freq (power save mode) and my application is low current in terms of the range of these parts. Input voltage is between around 2.7-3.6V (battery application) and output voltage of 3.0V which is what a buck+boost is targeted. Low Iq and lower switching frequencies are looked at as efficiency gains (counting constant loads as part of the "efficiency" story) for the TPS63036 vs the other alternatives. For apples-to-apples data, I'd like to see a TPS63036 Webench sim which allows for showing power-save mode enabled to compare against the efficiency of the 024 primarily. The output discharge of the 024 is not a key feature for my design - so this as a feature of the 024 is not "interesting". The 024 as the comparison mostly due to lower cost.