This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Power Monitoring for 24V lipo with only two outputs available...

Other Parts Discussed in Thread: BQ34110, BQ34Z100-G1

Hi..

I am using 24V 8 cell lipo battery ...

Problem :- Couldn't monitor each cell individual because of wrong fabrication . Can only monitor 24 v at a time . How to do this???

The idea i thought :- I thought of discharging the battery once and calculating the total power supplied and then dividing it by 100. Now i will monitor power and keep on decreasing he percentage when (totalpower/100) is supplied ..

Will i my idea work ??

Better solution if possible..