Hi,
Attached are two converters generated from WEBENCH, they appear to meet what I need. I'd like to lower the temperature (power loss) if possible without increasing the area too much, maybe a better power FETs. One question is the 1nF cap on the gate of low side driver. What is it used for, smoothing the drive?
I'd really appreciate it if someone knows the controller well to review the schematics and let me know any errors or anything I could improve. I added 2.5 ohm series resistors to the power FET gates, and optional snubber circuits to SW node.
Thank you!24V_5V_10A.pdf24V_12V_11A.pdf