This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27201A: Should the exposed bottom pad be connected to VSS?

Part Number: UCC27201A


I have a question in regards to the UCC27201ADPR, which is a WSON-10 package.  It is not clear in the datasheet, but should the exposed bottom pad be connected to VSS?

  • Leo,

    The exposed thermal die pad on the UCC27201ADPR (WSON-10) is not internally connected to VSS. The device will operate electrically even if the pad is not connected to VSS. However, the recommendation is to connect the exposed pad to a large thermal mass trace or GND plane to improve thermal performance.

    I hope this post helps answer your question. If it does, please press the "Verify Answer" button below.

    - Daniel