We are developing a circuit where we use the bq24610 to charge a 6S battery (25.2V fully charged). Our circuit is very similar to the application on page 26 of the data sheet.
We only modified the ISET1, ISET2, ACSET and VFB resistor dividers. We use the following resistors:
ISET1: VREF - 100k - MID - 8k2 - GND Setting for 1,25 A fast charge
ISET2: VREF - 100k - MID - 3k3 - GND Setting for 0,1 A precharge and termination
ACSET: VREF - 100k - MID - 33k - GND Setting for IDPM = 4,1 A
VFB: VBAT - 1,21MOhm - VFB - 110k - AGND Setting for 25,2 V
Our Inductor L1 is 10 uH/2A, Input voltage is 28 V. Following you can see a charging current curve we have measured. Additionally we measured the voltage at the battery during the Charge.
To this curves we have the following questions:
1) Why is the charging current already switched off at a current value of approximately 700 mA? We expect this switch-off later on at the ITERM threshold of 0,1 A.
2) Why is the battery voltage continuously rising? We would expect that a part of the curve should have constant battery voltage (Fastcharge Voltage Regulation Phase) by decreasing current.
Regards
Christian