Hi Team,
Our customer would like to know the output current threshold of the each mode.
Because, they are concerned about output ripple voltage in pulse skip mode.
-Pulse skip mode when IOUT less than ??mA
-Constant-frequency linear regulation mode when IOUT more than ??mA
[Customer’s conditions]
VIN=0.9V to 1.8V
VOUT2= 3.0V (VOUT1 is no connect)
IOUT2=0mA to 20mA
I understand that LinSkip switching threshold=7.5mA(typ) @ VIN=1.25V.
Does this current depend on VIN?
Could you please let us know this value if you have any information?
Regards,
Kanemaru