Other Parts Discussed in Thread: BQ25890, , TPS65218, TPS65010, LP3907, BQ24780S
In my system, these ICs are used:
bq25890 --- battery charging IC
bq27441 --- battery Gas Gauge
TPS650250 --- Power Management IC which provide 3.3V/1.8V/1.3V/3V LDO/1.2V LDO
The VCC_BATT of Li-Ion battery can vary from 2.75V to 4.2V.
When the battery supply power to the system through bq25890, the VCC_SYS = VCC_BATT.
So, when the VCC_BATT falls to below 3.3V, the TPS650250 can not provide 3.3V because it's a step-down DCDC.
Question: Does TI have any PMIC that can feed my needs? (1 buck-boost DCDC, 2 buck and 2 LDO)
Need 1 buck-boost DCDC, so that evern when the VCC_BATT falls to 2.75V, the PMIC can still provide 3.3V.
I looked through all the PMIC ICs, but didn't find any suitable chip.
Thank you.
Frank