This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A91: Output discharge time when en = low

Part Number: TPS7A91

Dear Team,

If you have TPS7A91 output discharge waveform showing the discharge time when en pulls low, please share with me. 

Thank you.

Regards,

Ting

  • Hi Ting,

    The discharge time will be application specific.  Factors that influence the discharge time include the output voltage, output capacitors, and the load current.  When TPS7A91 is disabled, a active discharge resistance of 250Ohms helps the load discharge the output capacitors.

    Very Respectfully,

    Ryan