This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23861EVM-612: About Ethernet switch for Alternative A application

Guru 19655 points
Part Number: TPS23861EVM-612
Other Parts Discussed in Thread: TPS23861

Customer is evaluating TPS23861EVM.

If customer use Alternative A connection, Is TPS23861EVM-612's EtherIN connect to the catalog Ether switch no problem? 

Or, is it need to use specific Ether swich? 

Best regards,

Satoshi

  • Hi Satoshi,

    Yes. TPS23861 supports Alternative A. TPS23861EVM-612 has 4 .at 30W ports on the left and they are wired as Alternative A.
    And it also has 2 high power ports on the right. These 2 high power ports are wired with 4 pair (both Alt A and Alt B are wired). Thanks.

    Best regards,
    Penny