Dear TI Team,
I had posted in one of the other threads regarding this. But since that one has been marked as answered, I'm opening a new one.
In my application, there is a ripple of about 1kHz in the TPS54202 Output. The amplitude is about 40mV p-p
I tried adding a phase boost capacitance (in parallel with the top feedback resistance). The ripple goes down as capacitance increases.
At about 10nF, the ripple is almost gone. Is this OK? The datasheet recommends adding only a few pF.
Will the loop stability be compromised in any way as the components age?
Circuit Parameters:
Vin - 18V
Vout - 12V
L - 47uH
C - 47uF - Aluminium Polymer
Cap ESR - 25mOhm @ 100kHz.
Tested Load: 1.5A
Measured Ripple Voltage(p-p): About 40 mV without phase boost cap.
Thanks in advance,
Vikram