Hello team,
I am supporting an application where WEBENCH suggests using a 33 µF Panasonic POSCAP tantalum capacitor for the output capacitor for LM2674M-5.0, the output voltage will be 5.0 V and output current around 250 mA and none of the alternate capacitors options seem to be ceramic capacitors they are all are either tantalum or aluminum.
Would you have any recommendation or considerations on using the ceramic capacitors with LM2674?
Two (2) 22 µF, 16 V Ceramics on the Output (TDK 445-3955-2-ND).
One (1) 4.7 µF, 25 V Ceramic on the Input (Murata GRM21BR71E475KA73L)