Hi team -- Is there anything about the following application that would preclude reliable operation (SOC,SOH accuracy, optimization, golden image production, etc) ?
Battery: LION K2 Energy LFP26650
Current boudaries: 90-100A discharge (max), 40-60A discharge (average use), 3A charge
Sense Resistor Value: 0.0005 ohms
We have been working on and testing a number of other applications using an OPAMP interface to mimic 0.0015 ohms to 0.0025 ohms to the BQ with some success, using the physical sense resistor value of 0.0005 ohms. We now have an application opportunity that can't afford to support any active components beyond the BQ core due to power budget in a long-term shelf-storage scenario.
thanks.