Hello,
I am using BQ27742-G1 fuel gauge with two INR18650-25R parallel cells and trying to read the power drawn from the battery. I am using the data command AveragePower() 0x76 and 0x77, but I am getting different values of power after two seconds or so. So, does it actually reads the instantaneous power? If not, over what time interval does it averages the power? And what is the sampling rate? I am bit confused because the command name is AveragePower(), but it is providing instantaneous values of power.
Please help to sort this out.