This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5165-Q1: loss of the IC itself

Part Number: LM5165-Q1


Hi,

We are checking the loss of each device on the circuit.
Is there data on the loss of the IC itself?
(Within the entire operating temperature range)

(specification)

VIN: 6 - 18V
VOUT: 5 V
IOUT: 0.1 A MAX
SW: COT, 230 kHz


VIN: 18-23V
VOUT: 5 V
Iout: 0.07 A MAX
SW: COT, 230 kHz

Best Regards,