This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610: Fuel gauge C/C++/Arduino drivers?

Part Number: BQ28Z610


Hello E2E community,

We are trying to build a prototype with the BQ28Z610 and an Arduino at our school.

I was wondering whether there were any C/C++/Arduino drivers available for monitoring a 2 cell Lipo?

Any help would be greatly appreciated.

Thanks,

TSI

  • Hi, 

    Not aware of any Arduino drivers....

    The BQ28Z610, as well as the rest of TI's fuel gauges use typically the I2C or/and SMbus protocol communication. So your device or microcontroller should be capable of either I2C or/and SMBus communication to read/write with the device. The BQ28Z610 specially uses 400kHz I2C Bus communication line. 

    Not too familiar with configuring the Arduino for I2C bus communication but this could help, playground.arduino.cc/.../WireLibraryDetailedReference

    Hope this helps,