This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5050-1: Can this part (and/or the LM5051) be used to implement an ideal bridge diode circuit

Other Parts Discussed in Thread: LM5051

I have to rectify an AC voltage of 14.5Vac (+10/-15%) at nominally 50 or 60Hz.

Currently I am using 4 x dual Schottky diodes (common cathode), in a bridge configuration.

I am using very low Vf diodes with a combined 70A If(avg).  In practice, with the current heatsink,
long term average currents above 50A raise the heatsink to temperatures above 100C
(25C ambient).

I would like to build a full MOSFET H-Bridge instead.

Can the LM5050 and/or LM5051 be used to turn 4 banks of MOSFETs into 4 x ideal diodes?
I envision that each MOSFET will be paralleled.

Assume I have all LM5050s (and/or LM5051s) separately powered from a voltage source of 20V,
derived independently from the same ac power, but with a bridge made with relatively low current,
low reverse leakage current, and very low Vf schottky diodes.  [with sufficient capacitance that the
droop between half cycles is less than 100mV - smoothing cap of 5 x 1000uF]