Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51003: Design and PCB recommandations

Part Number: BQ51003
Other Parts Discussed in Thread: PMP11311, TIDA-00668

Hi, 

I'm working on a design based on BQ51003 with a low Icc due to usage of a  small battery (60mAh) : high constraint about PCB size : very small.

I'll use a 4 layers PCB, but after reading documentation and have a look on reference design, I've few questions : 

- PCB thickness : 0.8mm possible? or not recommanded? with the small Icc not necessary to use 1.55mm?

- layer thickness equal 0.036 mm (Tpo, Mid1, Mid2, Bot)

- about via in Pad for BGA footprint :

hole size 0.152mm, diameter =0.254mm ?

via tenting on the bottom mandatory

is it necessary to fill via?

I can't find these informations in reference design, thanks for your help, recommandations and feedback

Best regards

  • Hi SG_34

    You are asking a PCB design question, I am not the best resource for this question. For a BGA part like this it is best to consult your CM that will build the device.

    The problem with an open via will be wicking of the solder away from pad. All my designs have the vias closed to prevent this.
  • Hi Bill,

    I follow reference design TIDA-0031, PMP11311 & TIDA-00668

    On these 3 designs, all vias on BQ51003 are on pad, tenting on bottom side, hole size 0.152mm and diameter =0.254mm

    Do you think I can design with a PCB thickness of 0.8mm, with clearance =150µm

    To avoid wicking, via tenting on bottom side is enough?

    Thanks for your support

    Stephane