This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5161: Is it possible to adjust the current limit threshold or the current limit off-time of LM5161?

Part Number: LM5161
Other Parts Discussed in Thread: LM5017

Hi experts team,

One of my customer is tryng to use our LM5161 as a buck converter.

Customer want to do more strict current limit (1A or even lower) than LM5161's 1.6A CL. I think seems only 2 ways to achieve this, one is to make current limit threshold lower, one is to make the current limit off time longer. but seems our current limit threshold and the CL off-time are fixed.

Is it possible to change the threshold and the off time using some external circuits? OR any recommend solution?

If we have, could you please share to me or send me email: joel-li@ti.com

Thank you!

Joel