Other Parts Discussed in Thread: LM43603, LM46002
Hi Team,
My customer got a LM53603 EVM and have a question related to switching frequency.
Customer changed the Vo voltage to 8V on the EVM, the load current is around 2A. When he tried to lower the Vin to around 8.5V ~ 9V. The switching frequency supposed should be maintaining at 2.1MHz(FPWM pin is connected to high to set device at forced PWM mode). But he found the Fsw is changed to 1MHz.
Please could team help to provide your comment on this phenomenon.
Thanks very much.
Vincent Chen