Other Parts Discussed in Thread: TPS61291
Hi Ti,
I'm looking for a buck-boost solution with a bypass mode. Below are the required specs.
•Minimum input voltage level: ~2.0V to 4.2V
•Efficiency: ~90% @ 100mA
•Max output current: ~500mA
•Quiescent current in bypass mode: <1μA
Please advise whether TPS63001 is able to do it with some tweaks? Or you may propose another solution. Thanks.