Other Parts Discussed in Thread: LM3409HV, LM3409, TPS92515, TPS92515HV
In this modification, I replace the R6 to increase the switching frequency. I do not want use the EN pin to do the shunt pwm dimming. Hence, I make a little modification by adding 2 external diode to preventing the coff being completely discharged. However, when I feed in the external pwm signal to drive the Q3, the switching is messed up. It did not switch properly (sometimes 30% on, 50% on, 20%on). I also notice that the formula to calculate the Roff2 is different between the and
For this case, I am using the LM3409HV datasheet's formula.
Also, I have doubt regarding the Rds(on) value that I should plug in into formula. In this case, I am choosing the Q3 Rds(on) value which is 19mOhm.
The Roff2 from LM3409HV vs LM3409HVevm is differ so much.
In my opinion, the Roff2 should be calculated with the same formula off Roff1, but changed the Vo to Vdd (8.3.2.2 Controlled Off-Time equation: 6). So the Roff2: ~13200ohms.
Thanks,