Other Parts Discussed in Thread: BQSTUDIO
Hi, I am currently using BQ27546 and integrated into device with small battery 165mAh 3.7V (Charging voltage 4.2V). I have update the data flash with Q_cell_max = 165, CC Gain is set at 19 mOhm. The other setting is set as default in BQ27546 technical reference document http://www.ti.com/lit/ug/sluub74/sluub74.pdf