Hello,
I am looking for a USB-C battery charger that has the following requirements:
- charge single cell Li-ion cell (4.2V)
- 500mA max charge current
- JEITA compliant
- low cost
Linear charger is ok, since we plan to charge at 250mA. Separate power path for the system would be great, but not required.
I saw the selection table:http://www.ti.com/litv/pdf/slua659 , and noticed none of these chargers in the table has connection to the D+, D- USB lines to sense power adaptor (>100mA source). BQ2405 does.
Do you have a other charger that connects to the D+/D- lines and also has separate power path to the system?
Thank you for help!