Tool/software: Code Composer Studio
Hi,
I am using piccolo-2000(28027F) as a host for the BMS IC BQ76PL455A-Q1. VIO pin of the Bq76pl455a-q1 ic is powered by the same power supply as of host controller ie. 3.3V.
but when i monitor the waveform during the UART communication of the ic and the host controller. the RX of IC signal has 3.3V peak to peak( min:0 and Max:3.3v) and TX of IC has 2.0v peak to peak (Min: 1.4 Max:3.3v)
Attached is the screenshot of monitored signals in oscilloscope for BQ76pl455a-q1 ic pins
channel 1- yellow - TX
channel 2- blue- RX
My Question is why am i getting different logic low levels for the TX & RX