Other Parts Discussed in Thread: TPS54202,
Hallo,
Kindly help.
Regards,
Surjit
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Thank you for your reply. The Input is +12V at PVIN and output is +11V at TP2, could it be due to voltage stored in C409 and C410? that current flow inside the IC when I start the input supply (0-12V)?
or It could be ESD? because +11V is connected to I/O through a fuse.
Is this IC short circuit protected?
Regards,
Surjit
Hi Luke,
Thank you, I will upload the waveforms as soon as I replace failed IC. L403 = WE-LHMI-74437349033, C409 and C410 = GRM32EC81C476KE15L
I set the Vsense so to get +11V output, with input at PVIN = +12V, I achieve +11V at PH (So IC works fine). But due to some reason (after some time) I found output terminal PH went to Ground (Could be internal MOSFET failed).
I have checked all possiblity but could not find possible cause Same issue with 3-4 ICs.
Please help, if you find any issue.
Regards,
Surjit
Hi Surjit,
The MLCC DC bias is exactly a little bigger, but it should not cause the chip damage.
Some query confirm with you:
1, As you said "I have not use a resistor at PH because I may draw 1-2A current, but I have used a Fuse." , so what's the reistor you mean? and where is fuse you used? we can't see the fuse in you schematic.
2, How the damage happen? during power up or...?
3, Did you try to disconnect the Vout with I/O loading, just test the converter to check if is still damage?
And also If we want to check why it is damaged, better we should catch some waveforms while the damage happen.
Catch waveform about V-PH(with full bandwith, >500MHz is better) and Vout, also check inductor current waveform if you can.
Regards,
Yuchang
Hi Yuchang,
I have updated the drawing, I have a load as LEDs and at I/O is also a Load (Kohm). Cause of damage I have to find out (possibly during power up).
I will try 3rd point now, I have used 3.3uH inductor but my current requirement is less. could this be a reason?
I have checked damaged IC, low side MOSFET is damaged (High side MOSFET still functional).
I will upload the wwaveforms after receiving new IC today.
Kindly looking for your reply.
Regards,
Surjit
Hi Surjit,
I would like you to check whether the IC will be damage without any loading.
if not damage, and then you can add loading with E-load to check when the chip damage and catch waveforms.
Regards,
Yuchang