Battery Monitor team,
We have a customer debugging a problem with the bq76940. The bq76940 is in Normal mode (based on REGOUT being 3.3V), and it gets into a state sometimes when there is no response on the i2c. Still trying to work out the exact sequence that leads up to this since it doesn’t happen often. Is there a way to reset the logic on the I2C slave interface of the bq76940 without fully removing the power?
Thanks,
Darren