In SLUUA65B–April 2014–Revised May 2016 the TRM for the BQ28Z610 the last sentence in the paragraph at the top of section 12.1 Standard Data Commands
is "Data RAM is updated and read by the gauge once per second." Does this mean that the part updates its data ram with new readings once per second?
If that is not what it means please elucidate.
There is a blog post that indicates that a minimum of 100us is required between sending a command and reading data from the part.
Is this the minimum time required for the part to wake up, process the command, and begin returning the data?
Is there a maximum time required for this to occur?
Thanks.