This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78PL116: *.aux file generation for a 16S battery

Part Number: BQ78PL116
Other Parts Discussed in Thread: BQ78PL114

Dear all,

I'm presently setting up a new 16S battery. I'm at the point now to do prepare the "Aux File Data Collection Run".

In the description how to setup the data log file  (application report "Chemestry Selection for bq78PL114" / SLUA505B) it says
to choose the default file "characterize_12cell.dlog" for the data collection run.

This file however is just configuring the data collection of voltages and temperatures for 12 cells, not for 16 cells.

With the implemented tool in bqWhizzard, the creation of a new dlog-file to cover all 16 cells is not possible as the maximum
allowed number of log definitions is limited to a maximum of 29.

Having 16 cells means 32 entries for the voltage and temperature logs alone. Adding the" Tick", "Current", "Pack Voltage",
"Relative State of Charge" and "Pack passed current" as required for a positive data aquisition run, this  will result in a total of
37 entries which neither is possible to create with the implemented tool nor is accepted by bqWhizzard when created manualy
in a text editor.

How can I overcome this limitation?

Anyone out there who already has successfully run an aux file generation for a 16S battery?

Thanks,
Marcus