Hi team,
My customer is testing TLV62569 EVM , 5.2V input, 0.9V output, 1A load.
and now we found the peak-peak noise on Vin pin is about 1.64V, maximum Vin is about 5.82V. that means if we use 5.5V input voltage, the maximum input voltage will exceed 6V. I notice that the maximum Vin tolerance is 6V, shown in datasheet. will this influence the performance of TLV62569.
Also, I notice that we have AC specification for SW, which is 9V/10ns,could you kindly provide the AC specification for Vin? Thanks for supporting.
Best,
Luke