Hi, team.
My customers are trying to design using UCC28070.
So, I got some question at this from customer.
Please tell me about it.
<Question>
①-1:How do you decide the optimum value of the peripheral parts of the Current detection ports (CSA, CSB)?
(Answer example 1: When VPKLMT = 3.3 V, average voltage of VCSA / VCSB is _ _ V and load current flows by _ _ A)
(Answer example 2: VPKLMT = 3.3 V, IOUTLIMIT = _ _ A, VCSA / VCSB can be decided by expression _ = _ _)
①-2: Is it OK that is to feedback from VREF by "VPKLMT = 3.3V"?
(Because it is a specification that VPKLMT can change, this pin also does not know whether 3.3 V is optimal)
②In the application Diagram, the current sense is sensed with an AC signal using a transformer, but is it possible to design by detecting by using a shunt resistor "M1 / M2 's above or below"?
③Is the input signal to the system usable at 42 to 69 Hz (50/60 Hz ± 15%) at AC?
④When disabling the operation of IC (UCC 28070), which terminal should be controlled?
Best regards,
Masumi Sekiguchi