Other Parts Discussed in Thread: UCC28220
Hi All,
Two DC-DC Converters( Analog Based) are used in parallel to Meet load of 2.5kW, 48V/28V output voltage, & I am intending to use UCC39002 Load share IC.
1. Is UCC39002 Compatible to work with UCC28220 Interleaved Forward Converter IC?
2. I intend to control the error output of UCC39002 by mapping with UCC28220 so that PWM is regulated according to shared load between two separate DC-DC Converters.
If yes, then how can it be done. Because UCC28220 already has Current Sense Pins for Current Feedback and CTRL Pin for Voltage Feedback & PWM is generated accroding to loop correction in it.
Thanks & Regards
Sai Charan