Part Number: TPS61099
Hello all,
The datasheet for the TPS61099 device, in the Pin Configurations section (page 3) states:
"Voltage feedback of adjustable output voltage. Connect to the center tap of a resistor divider to program
the output voltage. Connect to GND pin for fixed output voltage versions."
But in section "9.2.1.1.2 (page 13) Programming the Output Voltage" It states:
"For fixed output voltage versions, the FB pin should be connected to the VOUT pin directly. The TPS61099x offers diverse fixed voltage versions, refer to Device Comparison Table for version details."
Please clarify which of these statements is correct