Other Parts Discussed in Thread: 66AK2G02,
I am doing a 66AK2G02 design based on the EVM2KG. Do you have guidance on what to do with unused pins or unused functions of the TPS659118?
For example, in the EVM2KG, there are pairs of capacitors on the inputs and outputs of regulators that are not actually connected to anything in the circuit: VCC7/VRTC, VCC4/LDO5, VCC3/LDO6-8. Are all these capacitors really required?
I infer that nothing needs to be connected to VBACKUP, because the EVM has only a jumper there and ships with nothing installed on the jumper.
Regards,
Debora