Hi
Could you help
I have a problem with the "Charging Status Indicator".
My manipulation is the following :
The board is configured with USB, the battery is connected ( OTG is disabled, Charging is enabled).
I connect the external power supply.
I disconnect the external power supply.
A this moment the bit for the detection stayed at "1" (0xAC, bit 3).
PMID is at 4V and the USB is at 4V.
If I disabled and enabled the charging, everything goes well. But if I connect and disconnect the external power supply I find again the problem.
I don't know if this issue could come from the capacitor used on power supply.
Thanks for your support.