Other Parts Discussed in Thread: BQ25703A
Hi,
Im testing the BQ24780S EVM and seeing the datasheets looks like it is able to do this but I can't obtain any good result...
I've changed the resistor divider of ACDET to obtain 2.5V with 12V at input, but this is not enough... ACOK needs also VCC>BAT so I think I can't get 12Vout with 12Vin and 12V battery.. but maybe there is a way to solve this like changing the battery to a 9V battery, the problem is that I cant get 12V at output, only Vin or Vbat when Vin is off. Seems like no converter is running, but the charge inhibit (0x12[0]) is 0 and ChargeCurrent (0x14), ChargeVoltage(0x15) and InputCurrent(0x3F) are loaded.
Can help me anybody?
Thanks a lot