Part Number: BQ24765
The Battery-Charger-IC-Products selection page shows the BQ24765 is used with 2 to 4 Lithium cells. The data sheet also indicates the same 2 to 4 cell criteria. The part description shows the Battery Charge Minumum Voltage to be 1.024 volts. That would seem to indicate the BQ24765 could also be set up to charge 1 Lithium Cell. In addition, at the bottom of page 1 of the BQ24765EVM user's guide, I see that the EVM Features includes User selectable 1 cell, 2 cell, 3 cell, and 4 cell.
Can the BQ24765 be used to control charge into 1 Lithium cell as well as the 2 to 4 in the data sheet?
dpk