This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5122: No bypass mode at input supply great than target output

Part Number: LM5122

Hi Expert,

Need you to clarify below condition why the bypass mode not operated.

Condition: Vin=16V and target Vo=12V

Within the 16Vin applied,the Vo is equal to Vo now.We see the UVLO,SS and VBST are active to expected rating.But not see any high side mosfet driver signal.

But if we apply 10Vin to get 12Vo firstly.Then increase the Vin to 16V.The 100% high side driver will had.

Pls advice why the bypass mode not worked here.

Best regards,

Eric Lai

 

Field Application Engineer

Texas Instruments Taiwan Limited

O: +886-2-2175-2582

M: +886-909-262-582

E-Mail:Eric.Lai @ti.com