This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS74401: help check the design

Part Number: TPS74401

Dear Sir

Please help check the attached schematic and give some advice.

thanks

StarPowe Design.pdf

  • Please allow a short delay due to the US Holiday.

    Very Respectfully,
    Ryan
  • Hi Star,

    It appears that there are two TPS74401 (U19 and U22).  Not all voltages are shown on the schematic.  Both appear to be okay so long as PL_VIN satisfies the Vbias dropout requirement (2.82V or more would cover it under all conditions).

    There does not appear to be a pullup resistor for PG for U19.

    It appears that the recommended resistor divider is used for U19 for a 1.2V rail; however, the recommended resistor divider is not used for U22:

    Neither U19 or U22 have a localized input capacitor.  The recommended input capacitor is 1uF.

    Very Respectfully,

    Ryan