Other Parts Discussed in Thread: UC2843, LMG5200
Hi all,
I'm working on an adjustable (0 - 60VDC with 0.1VDC steps) offline SMPS. The topology will be 2-sw forward and I'm planning to use UC2843 as the controller.
Since the output is adjustable and the minimum output voltage is 0.1VDC, the minimum duty cycle will be less than %0.1 (calculated from Np / Ns = Vi x D). So the minimum pulse width will be less than 10ns!
According to datasheet, rise- and fall-times for the output section are given as 50ns typical and 150ns maximum. For 10ns of pulse width, gate drive signal will be triangular (and of course will have lesser amplitude), so I think that the MOSFET cannot be driven properly. Am I right?
What should I do?