Hello,
Our customer would like to set the output current as 20mA(min) and 2A(max).
In order to avoid the flicker phenomenon, I would like to use Analog Dimming.
However, since the IADJ range is 140mV to 2.25V, we can't achieve 2A(max) and 20mA(min) with analog dimming.
Thus, I would like to set to the following settings to achieve this requirement.
Rcs=0.075ohm, VIADJ=140mV, then ILED will be 133mA, and PWM duty dimming 15%.
Then I have the following questions.
(1) PWM frequency
Could you please let me know the maximum PWM frequency for this case?
How much should I set the PWM dimming frequency to avoid flicker?
I want to prevent movie shooting from being affected.
Current Fsw setting is 390kHz.
(2) Analog dimming accuracy at low voltage setting
If VIADJ is set to 21 mV, 20 mA is set with Rcs of 0.075 ohm.
What is the current accuracy in this case?
(3)Other method
Could you please let me know more better way for this requirement if there is?
Best Regards,
Ryuji