This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM27761: Combine Outputs of two LM27761 devices to get 500mA current

Part Number: LM27761

Is it possible to combine the outputs of Two LM27761 devices to get 500mA current?

Design requirements are as below,

Vin   : 5v

Vout :    -1.8v

Iout :    500mA