Hi
When the system is in standby it draws only 0.5mAh from the battery.
This current is to small for the bq27500 v130 to measure so it has to be calculated by the fuel gauge.
This is not the case, when I use a configured .DFI file.
Dos it help to finish the cycling and the golden .DFI file?
Or is there any other parameter I can focus on?
Best regards
Emil