This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24650: Can BQ24650 could be used to Charge 14.8V 10Ah Lipo Battery?

Part Number: BQ24650

Hi,

I have few questions about BQ24650.

I read datasheet of BQ24650 it support Lipo batteries and MPPT algorithm. I have 14.8V 4S 30C battery and I would like to charge it with Solar Panel of 40W to 80W. Can I use BQ24650 for this purpose.I understand that I have to change Resistors to set MPPT Voltage and Charge current.

What could be the Max charging voltage and  current to charge 14.8V LiPo Battery? 

BQ24650 supports balanced charging? is it ok if I am not using balanced charging?

Reagrds,

Naveen