Part Number: LM78M
Hello,
I am using LM78M15 for one my circuit to convert the 24V DC input to 15V regulated output. As per datasheet the maximum input voltage is 35V.
My question is if the input voltage goes beyond 35V for a sec will the output voltage still regulate to 15V or is there any chances that the output voltage exceeds 15V?
Since I am asking this question is I am using this 15V to external encoder interface with 18V TVS protection(1500W). The TVS I am using is failing with short circuit mode and PCB tracks are damaging. The failure of TVS is observed frequently.