Part Number: TPS54620
Tool/software: WEBENCH® Design Tools
I have created a design using Webench, First I have selected switching frequency 200KHz, It suggests Inductor Value 4.5uH (Minimum) to 5.5uH (Maximum),
I can edit the lower Value 4.5uH to 1 uH and use 1uH part in Design, It updates the value a provides design File with similar characteristics.
Questions :-
1. Is it okay to use Inductor value less then recommended Value?
2. When I change the Inductor Value less, Why tool did not give me error message or recalculate designs based on new Inductor Value?