Hello,
I am using the TPS71733 LDO fixed at 3.3V but I am actually getting 3.92V.
I have a 0.1 and 1.0uF input ceramic caps. 1.0uF output ceramic cap and a 0.1uF noise reduction capacitor.
Input voltage is 4.975V from a TPS7B6950 supplied rail.
The diode footprint is included in the event reverse current protection was needed. In or out of circuit this does not change the output of the TPS71733.
The trace that goes to the left of the output goes to a programming header for programmer supplied voltage.