This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: CHG and DSG MOSFETs not turning on properly

Part Number: BQ4050

I am using a bq4050 circuit along with a standalone charger. I am using 3s1p pack for initial studies. The pack voltage is presently around 9.9V. I find that the DSG mosfet is not turning on at all. I have wired up the circuit as per the application schematic.

Voltages at :

CHG pin = 5.3V

DSG pin = 0V

I have connected both PTCEN and PTC pin to ground as I am not using this feature. This is the only change in my circuit compared to the application schematic. The EVM is working perfectly fine in my application.